Point of Operation Control Safety Light Curtains

Point of Operation Control (POC) safety light curtains are designed for finger, hand, and arm detection. These light curtains are placed close to the hazard, at the point of operation where personnel may frequently interact with the machine.

Bulletin 450L GuardShield POC Safety Light Curtains

450L GuardShield POC

Our Bulletin 450L GuardShield™ POC safety light curtains are unlike traditional safety light curtains, which are based on separate transmitter and receiver units. This next generation light curtain system features patented technology, which allows each transceiver to be used as a transmitter or receiver via an innovative plug-in module. This advanced technology greatly reduces stock and provides a flexible, cost-effective safety solution.


Bulletin 440L Guardshield POC Type 4 Safety Light Curtains

440L Guardshield POC Type 4

Our Bulletin 440L Guardshield™ POC Type 4 safety light curtains are applied in applications where a formal risk assessment has determined that the hazard poses a moderate to high risk of operator injury.


Bulletin 445L Guardshield POC Type 4 Micro 400 Safety Light Curtains

445L Guardshield POC Type 4 Micro 400

Our Bulletin 445L Guardshield™ POC Type 4 Micro 400 safety light curtains are economical three-box safety light curtains in a small housing. Designed for use in benign industrial environments (IP54), this light-duty system is targeted to the semi-conductor, micro electronic and small assembly machine markets. We also offer these light curtains in cascadable configurations and in IP69K enclosures. The Micro 400 requires a dedicated controller such as the MSR41 for ON/OFF applications or the MSR42 for advanced safety functionality.


Bulletin 445L GuardShield POC Type 4 Safe 4 Safety Light Curtains

445L GuardShield POC Type 4 Safe 4

Our Bulletin 445L GuardShield™ POC Type 4 Safe 4 safety light curtains are economical two-box safety light curtains with ON/OFF functionality. These basic, guard-only operating mode safety light curtains have an integrated laser alignment system to simplify the alignment of each pair of light curtains. Visible laser beams are activated by touching the laser at the finger symbol on the front face of the light curtains.


Bulletin 440L and 445L Guardshield POC Type 2 Low Risk Safety Light Curtains

440L and 445L Guardshield POC Type 2 Low Risk

Our Bulletin 440L and 445L Guardshield™ POC Type 2 Low Risk safety light curtains are applied in applications where a formal risk assessment has determined that the hazard poses a low risk of operator injury.