Cable Pull Switches

Cable Pull Switches have a steel wire rope connected to latching pull switches. Pulling on the rope in any direction at any point along its length will trip the switch to cut off the machine power. Select from our Lifeline™ Rope Tensioner System (LRTS), Lifeline 3 cable (rope) operated emergency stop device, Lifeline 4 cable/push button operated system, and our stainless steel Lifeline 4 cable/push button operated system.

Bulletin 440E Lifeline 3 Cable Pull Switches

Lifeline 3 Cable Pull Switches

Our Lifeline™ 3 Cable Pull Switches are cable (rope) operated emergency-stop devices designed to meet the stringent requirements of ISO 13850 (Safety of Machinery—Emergency Stop Equipment). The Lifeline 3 system can be installed along or around awkward machinery and provides a constant-access emergency-stop facility.


Bulletin 440E Lifeline 4 Cable Pull Switches

Lifeline 4 Cable Pull Switches

Our Lifeline™ 4 Cable Pull Switches can be installed along or around awkward machinery such as conveyors and provide a constant emergency stop access. The system includes a rope status indicator and emergency stop button mounted on the switch lid. This switch is also available in stainless steel 316 and is suitable for external use, applications where there are hygiene requirements, and other situations where a level of corrosion resistance is required.


Bulletin 440E Lifeline Rope Tensioner System

Lifeline Rope Tensioner System

Our Bulletin 440E Lifeline Rope Tensioner System (LRTS) is a unique cable (rope) tensioning system which enables quicker installation of cable actuated systems. The LRTS can also be used for applications other than cable actuated emergency stop systems.