Emergency Operators include enabling switches and cable pull switches. Our Lifeline™ series includes cable emergency-stop switches and cable actuated emergency-stop switches.
![]() | Cable Pull Switches have a steel wire rope connected to latching pull switches. Pulling on the rope in any direction at any point along its length will trip the switch to cut off the machine power. Select from our Lifeline™ Rope Tensioner System (LRTS), Lifeline 3 cable (rope) operated emergency stop device, Lifeline 4 cable/push button operated system, and our stainless steel Lifeline 4 cable/push button operated system. |
![]() | Our enabling devices are manually operated control devices used in conjunction with a start control. Our three position enabling switch can be used as part of the conditions required to allow safe working inside a machine guard. |