Our gSE vibration modules measure conventional and g Spike Energy (gSE) vibration. gSE is a signal processing technique providing an accurate measure of the energy generated by transient or mechanical impacts.
![]() | The XM® 122 gSE Vibration Modules measure both conventional vibration and g Spike Energy (gSE). gSE is a signal processing technique that provides an accurate measure of the energy generated by transient or mechanical impacts. These modules are ideal for monitoring motors, pumps, fans, and gearboxes that are fitted with rolling element bearings and where continuous, real-time, protection is not required. |