Our condition monitoring sensors support vibration and position measurements for most applications in environments ranging from the benign to the extreme with respect to temperature and hazardous locations. We offer two families of eddy current probe systems for applications that require measurements of the dynamic and/or static displacement of the target relative to the mounting fixture. We offer a comprehensive family of accelerometers for when common acceleration or velocity measurements are needed.
![]() | Our 9000 series accelerometers are general-purpose sensors that measure vibration on industrial machinery. We offer a broad selection of sensors that provide capabilities such as low frequency, high frequency, high temperature, and velocity output. |
![]() | Our eddy current probes are non-contact pick-ups that satisfy the American Petroleum Insitute (API) Standard 670 requirements. The sensors are non-contacting eddy-current type transducers that measure the dynamic and/or static displacement of a target surface, such as a shaft, relative to the mounting fixture, such as a bearing housing. We offer accessory items such as tachometer signal conditioners, linear differential variable transformers, rotary potentiometers, and hall effect speed sensors. |