Our packaged vibration monitors are pre-assembled vibration monitoring systems. Each package includes a dynamic measurement module or a gSE vibration module, an expansion relay module, and a front panel display.
![]() | The XM® 720 Packaged Vibration Monitors include an XM-120 Standard Dynamic Measurement Module, an XM-441 Expansion Relay Module, and a front panel display. These standalone solutions monitor the condition of fans, pumps, blowers and other essential machinery. |
![]() | The XM® 721 Packaged Vibration Monitors include an XM-121 Low Frequency Dynamic Measurement Module, an XM-441 Expansion Relay Module, and a front panel display. These standalone solutions monitor the condition of fans, pumps, blowers and other essential machinery. |
![]() | The XM® 722 Packaged Vibration Monitors include an XM-122 gSE Vibration Module, an XM-441 Expansion Relay Module, and a front panel display. These standalone solutions monitor the condition of fans, pumps, blowers and other essential machinery. |